Recommendations

Access Recommendations in FMEA

About This Task

Procedure

  1. Access the Failure Effect for which you want to access recommendations.
  2. Select the recommendation that you want to access.
    The datasheet of the recommendation appears.
    Tip: For information about additional options available when working with recommendation records, refer to the Recommended Actions section of the documentation.

Add a Recommendation

Procedure

  1. Access the Failure Effect for which you want to add recommendations.
  2. Select .
    The new recommendation datasheet appears.
  3. As needed, enter values in the available fields.
  4. Optionally, to include action information in the recommendation, select the Action Information tab, and then, as needed, enter values in the available fields.
  5. Select Save.
    The Recommendation is saved.