Troubleshooting Scenarios

Troubleshooting Scenarios

The following topic can help you troubleshoot issues that you may have with the Rounds Designer module:

Route Takes a Long Time to Load

Description

Route takes a long time to load in Rounds Designer.

Cause

This may occur if the Route size is very large.

Solution

  • Route sizes should not exceed 250 checkpoints (including conditional checkpoints). This ensures optimum performance of the Route in Rounds Data Collection (RDC). It will also reduce the overhead on the server by avoiding upload of large numbers of readings on a single Route.
  • The maximum number of checkpoints for a single condition should not exceed 15.