Automated Data Loader Service Installation
Install Automated Data Loader Service
The Automated Data Loader service required for integrating to APM using Automatic Data Loader (ADL) is configured as part of the Southbound Service installation. To use only the ADL, execute the Southbound Service and Postgres installation only. You do not require a remotely managed runtime environment for ADL to function.
Create ADL directories
The following table lists the directories that must be created when using the ADL.
Considerations:
- The folders must be created in the directory specified in the southbound configuration file (see ADL Configuration).
- Create the directories only for the Data Loader types that are in use.
Note: By default, all the Data Loader Types have the same processing priority of 99 (prefix). This can be changed to get precedence in the processing. For example, 01˜FamilyDataLoader.
Data Loader Name | Folder Name |
---|---|
Family Data Loader | FamilyDataLoader |
Equipment and Functional Location Loader | EquipmentFunctionalLocationLoader |
Taxonomy Data Loader | TaxonomyLoader |
Work History Loader | WorkHistoryLoader |
Production Loss Analysis (PLA) 1 - Admin | PLAAdminBatchDataLoader |
Production Loss Analysis (PLA) 2 - Event | PLAEventBatchDataLoader |
Production Loss Analysis (PLA) 3 - Plan | PLAPlanBatchDataLoader |
Root Cause Analysis (RCA) | RCABatchDataLoader |
System Reliability Data Loader | SystemReliabilityBatchDataLoader |
Asset Criticality Analysis (ACA Checklist) | ACACheckListDataLoader |
Asset Criticality Analysis (ACA) | ACAMatrixDataLoader |
GIS Data Loader | GISDATALOADER |
Policy Instance Data Loader | PolicyInstanceBatchDataLoader |
Role Data Loader | RolesDataLoader |
Rounds Allowable Values | AllowableValuesBatchDataLoader |
Rounds Readings | ReadingsBatchDataLoader |
Rounds Routes | RouteBatchDataLoader |
Rounds Templates and Template Groups | TemplateBatchDataLoader |
Inspection Management (IM) Assets | IMBatchAssetDataLoader |
Inspection Management (IM) Functional Location | IMBatchFLDataLoader |
RBI Components To TML Groups Relationship | RBITMBatchDataLoader |
Risk Based Inspection (RBI) 580 | RBI580BatchDataLoader |
Risk Based Inspection (RBI) 581 | RBI581BatchDataLoader |
Risk Based Inspection (RBI) Corrosion Loop | RBICorrosionLoopBatchDataLoader |
Thickness Monitoring (TM) Equipment | TMBatchAssetDataLoader |
Thickness Monitoring (TM) Functional Location | TMBatchFLDataLoader |
Thickness Monitoring (TM) Piping Equipment | TMBatchPipingAssetDataLoader |
Thickness Monitoring (TM) Piping Functional Location | TMBatchPipingFLDataLoader |
Generation Availability Analysis (GAA) GADS Amplification Codes | GAAAmplificationCodeDataLoader |
Generation Availability Analysis (GAA) GADS Cause Code | GAACauseCodeDataLoader |
Generation Availability Analysis (GAA) Events | GAAEventsDataLoader |
Calibration Management | CalibrationBatchDataLoader |
Hazard Analysis | HazardAnalysisBatchDataLoader |
Asset Strategy Management (ASM) | AsmDataLoader |
Asset Strategy Management (ASM) Template | AsmTemplateDataLoader |
Failure Modes and Effects Analysis (FMEA) | FMEAAnalysisDataLoader |
Failure Modes and Effects Analysis (FMEA) Analysis Templates | FMEAAnalysisTemplateDataLoader |
Failure Modes and Effects Analysis (FMEA) Asset Templates | FMEAAssetTemplateDataLoader |
Reliability Centered Maintenance (RCM) | RCMAnalysisDataLoader |
Reliability Centered Maintenance (RCM) Analysis Template | RCMAnalysisTemplateDataLoader |
Risk Matrix | RiskMatrixDataLoader |
GAA Wind Asset Hierarchy | GAAWindAssetHierarchyDataLoader |
GAA Wind Events | GAAWindEventDataloader |
GAA Wind Sub Group Capacity | GAAWindSubgroupCapacityDataLoader |
Rounds Pro - Picklist Dataloader | PicklistDataloader |
Rounds Pro - Route Master Dataloader | RouteMasterDataloader |
Rounds Pro - Step Dataloader | StepDataloader |
Rounds Pro - Step Conditions | StepConditionDataloader |
Rounds Pro - Step Template | StepTemplateDataloader |