Overview

About APM Connect

The APM Connect system provides the means to load data from the Industrial Internet of Things (IIOT) into APM.

The system uses data loaders and adapters to establish a data flow between APM and EAM systems, Field Service Management systems, and other assets. The APM Connect context file defines the communication path between the IIOT and APM.

Note: For information about the APM Connect versions corresponding to APM versions, refer to the APM Connect Version Compatibility Table.

APM Connect Next Generation ETL is the new integration tool in replacement to the existing technology stack. The new model provides for common workflow development, deployment, execution, and monitoring with remote management option.

You can ingest data to APM using one of the following methods:

Access the APM Connect Page

Procedure

In the Applications menu, navigate to ADMIN > Operations Manager > Connections., and then select APM Connect.

The APM Connect workspace appears.