Steps
On the left navigation menu, select Health, and then select Rounds Data Collection.
The RDC Overview page appears.
The tabs at the top of the page summarize Route information in various categories. You can select a tab to view one of the following sections:
Assigned Routes: Displays a list of Routes that are assigned to you. From this section, you can enable or disable offline access, or mark a Route done. The number on the tab indicates the number of Routes that are assigned to you.
Recommendations: Displays a list of all Recommendations. The number on the tab indicates the number of Recommendations.
This page also includes the following items:
The Device Settings button: By default, a mobile device must be connected to the network while you take readings. You can also take the readings offline by enabling offline access and setting the download horizon and sync interval with the device using this button.
The Scan button: You can use this button to scan the barcode of an asset or a location using the camera of the mobile device that is used for data collection.
Note: This button appears only if you are using the GE Digital APM mobile application.
The information on the RDC Overview page is related to the asset hierarchy level. You can set the hierarchy level either by selecting
Copyright © 2018 General Electric Company. All rights reserved.