To enhance data collection on small screen devices, such as mobile phones and small tablets, GE Digital APM automatically adjusts the page layout when you use Rounds Data Collection on any device with a screen less than 769px wide.
Supported Features on Small Screen Devices
The following features are not supported in Rounds Data Collection on small screen devices:
All other standard features of Rounds Data Collection are supported on small screen devices.
While the supported features behave in the same way when you are using a small screen device as they do when you are using a larger device, the following features are displayed differently:
As shown in the following image, the contents of the page are adjusted to fit a small screen device.
On a small screen device, the button you select to open the barcode scanner (
On a small screen device, the button you select to open the Device Settings window (
The Route Map pane
On a small screen device, the Route Map pane does not appear automatically when you access a Route for data collection. The button you select to view the Route Map pane (
Copyright © 2018 General Electric Company. All rights reserved.