In the upper-right corner of the page, select Scan.
The barcode scanner for your mobile device appears.
Using your mobile device, scan the barcode assigned to the Route or checkpoint that you want to access.
A window appears that allows you to navigate to the matching checkpoint or Route.
Select OK.
Results
If the barcode that you scanned is associated with a checkpoint on the current Route as well as a checkpoint on a different Route, the checkpoint on the current Route opens automatically.
If the barcode that you scanned is associated with a Route that is not the current Route, a window appears that allows you to navigate to the Route that you want to access.
If the barcode that you scanned is associated with a checkpoint on more than one Route but not on the current Route, a window appears that allows you to navigate to the matching checkpoint whose related Checkpoint Task has the earliest Next Date. If multiple checkpoints have the same Next Date, you can navigate to the first Route, sorted alphabetically, that contains the checkpoint.