This topic describes how to create a Checkpoint Condition and add it to a Route:
As a successor to a Lubrication Requirement for all types of Lubrication Requirements.
-and-
Steps
The Lubrication Requirement node for which the reading value triggers the conditional Lubrication Requirements to appear.
-or-
In the left pane, select
A new Checkpoint Condition is created, and appears below the selected Lubrication Requirement or Checkpoint Condition node.
On the upper-right corner of the datasheet, select
The Checkpoint Condition is saved. The Checkpoint Condition node displays part of the final condition statement, similar to the one shown in the following image.
If you want to create a new Lubrication Requirement, select New LR.
-or-
If you want to add a existing Lubrication Requirement, select Existing ML / LR.
-or-
The Lubrication Requirement is added to the Route, and a Lubrication Requirement node appears below the predecessor Checkpoint Condition. In the following image, you can see a new Lubrication Requirement node.
On the upper-right corner of the datasheet, select
The Lubrication Requirement is saved. The condition statement is complete.
Copyright © 2018 General Electric Company. All rights reserved.