Create a Checkpoint Using a Blank Datasheet

Steps

  1. Access the Route in which you want to create a checkpoint.
  2. In the left pane, select the node that should appear preceding the new checkpoint. If no nodes are present, proceed to step 3.

  3. In the upper-left corner of the pane, select , and then select New ML or New LR.

    A blank datasheet for the checkpoint appears.

  4. As needed, enter values in the available fields for a New ML or available fields for a New LR.

  5. Optionally, in the Schedule section, define a schedule for the checkpoint.

    Note: The checkpoint schedule is required if the Route does not have a schedule.

  6. On the upper-right corner of the datasheet, select .

    The checkpoint is created.

Copyright © 2018 General Electric Company. All rights reserved.