Configure Node Properties

Steps

  1. Access the policy that contains the node whose properties you want to configure.
  2. In the Design workspace, select the node whose properties you want to configure.

    The Properties window for the node appears. The following image shows an example of the Properties window for a Threshold Statistics node.

  3. If the Properties window contains a Name text box and you want to use a name other than the default name, enter a name for the node. For some nodes, the name that you specify also appears as the node label in the policy model.
  4. Define any input values for the node.
  5. Configure any additional properties that are specific to the node.

    Hint: For details about the properties that you can configure for each node, refer to the following sections in this documentation: Input Nodes, Condition, Logic, and Calculation Nodes, and Action Nodes.

  6. Repeat these steps for each node in the policy model.
  7. In the Policy section of the toolbar, select .

    The policy is saved.

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.