Add Nodes to the Model Canvas

Steps

  1. Access the policy to which you want to add nodes.
  2. In the Design workspace, in the section of the toolbar for the type of node that you want to add, select the button for the node and drag it to the model canvas.

    For example, if you want to add a Point Value node, on the Inputs toolbar, select the button and drag it to the model canvas.

    Hint: In each section of the toolbar, you can select the button to see additional nodes and to see what each button represents.

  3. In the location where you want the node to appear, release the pointer.

    The node appears on the model canvas and the Properties window for the node is displayed.

  1. In the Policy section of the toolbar, select .

    The policy is saved.

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.