To illustrate the different ways to define
input values, consider the following nodes and connections.
In this example, the Equipment Entity node is connected to an Equal Condition node. The Properties
window for the Condition node, therefore, allows you to select the Equipment family and one of
its fields. As shown in the following image:
- The icon appears
in the first input section, indicating that the input is defined by a predecessor node.
- The icon appears in the second input section, indicating that the input is a user-defined constant value.
Together, the Equipment Entity node and the Condition node to which it is connected indicate that
an email message should be sent when an Equipment record has a value
of A in the Criticality Indicator field.
Note:
You will use policy instances
to identify the specific record(s) whose values you want to use in the
policy. For the example provided in this topic, you would use a specific Equipment record in each policy instance that is
associated with the policy.