The following table outlines the steps that you must complete to deploy and configure this module for the first time.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Note:
Step | Task | Notes |
---|---|---|
1 | Define alternate search queries. | This step is required only if you do not want to use the baseline search queries. |
2 | Manage the types of Deviations in a HAZOP Analysis. To do so, add a code to the MI_HAZOP_DEVIATIONS system code table. | This step is required only if you want to add another value to the list of default values in the Deviation/Guideword list in the HAZOP Deviation datasheet. |
3 | This step is required only if you want to take advantage of the integration between the SIS Management module and Hazards Analysis. | |
4 |
Assign Security Users to the MI SIS Administrator or MI SIS Engineer Security Group. |
This step is required only if you want to take advantage of the integration between the SIS Management module and Hazards Analysis. |
5 | Review the Hazards Analysis data model to determine which relationship definitions you will need to modify to include your custom equipment or location families. Modify any relationship definitions as needed via the Configuration Manager application. | This step is required only if you store equipment and location information in families other than the baseline Equipment and Functional Location families. |
|
Assign Security Users to one or more of the Hazards Analysis Security |
This step is required. |
Copyright © 2018 General Electric Company. All rights reserved.