Add System Codes to a Table

Steps

  1. Access the System Codes and Tables page.
  2. From the System Tables section, select the System Code Table for which you want to add System Codes.

    The details of the table appears.

  3. In the System Code subsection, select .

    The Create System Code window appears.

    Create System Code window

  4. In the ID box, provide ID for the System Code.

    The ID must be unique and must not exceed 50 characters in length.

  5. In the Description box, provide a description for the System Code.

    The description must not exceed 255 characters in length.

  6. Select one of the option: Default or Active.

  7. Select Save to save the new System Code that you have created.

    The new System Code is added and appears in the System Code subsection.

Copyright © 2018 General Electric Company. All rights reserved.