The Exceptions and Tasks workspace appears, displaying the following sections:
Exceptions: Contains a list of Exceptions that are associated with the Change Project. For each Exception listed in this section, the following information appears:
<Exception ID>: The value in the Exception ID field of the Exception appears as a link, which you can select to access the selected Exception.
Status: The value in the Status field of the Exception.
Reference Document: The number of Reference Documents associated with the Exception.
Source: The value in the Question Text field of the Question, in response to which the Exceptions was created.
Above the Exceptions section, the number of Exceptions associated with the Change Project and the number of Exceptions in each Exception status appear.
Tasks: Contains a list of tasks that are associated with the Exception that you select in the Exceptions section. For each task listed in this section, the following information appears:
<Task ID>: The value in the Task ID field of the Operations Task record appears as a link, which you can select to access the selected Exception.
Assigned To: The value in the Task Assigned To field of the Operations Task record.
Start Date: The value in the Next Date field of the Operations Task record.
Interval: The value in the Desired Interval field of the Operations Task record.
Above the Tasks section, the total number of tasks associated with the Exception and the number of tasks in each task state appear.