MI MOC Exception Records

MI MOC Exception records store information about the Exceptions. For a Checklist added to the Change Project, when the selected Answer Option for a Question is associated with an Exception, a copy of the Exception created in MOC Application Settings is created. This topic provides an alphabetical list and description of the fields that exist for the MI MOC Exception family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Description Character Contains a description about the Exception. This field is populated with the value in the Description field of the MI MOC Exception record whose copy is being created.
Exception ID Character The identification of the Exception.

This field is automatically populated with a unique value.

Exception Type Character The type of Exception. This field is populated with the value in the Exception Type field of the MI MOC Exception record whose copy is being created.
Is Admin Setting Boolean Indicates whether the Exception represents a record created in the Application Setting.

This field does not appear on the datasheet.

This field is True if you created the record using the Application Settings for Management of Change.

This field is False if GE Digital APM automatically created the record as a copy of the Exception that you created.

Status Character Indicates the status of the exception.

This field appears as a list that is populated by the MI_EXCEPTIONS_STATE System Code Table.

Copyright © 2018 General Electric Company. All rights reserved.