This topic describes how to create a new Primary Event using one of the following methods. You can also copy a Primary Event.
Use this method when detailed information for an event is available.
Select the Events Under Review tab.
A list of Primary Events available in the database appears.
In the upper-left corner of the Events Under Review section, select
Note: You can also create a new Primary Event by:
The New Event window appears, displaying a blank datasheet.
Select
The new Primary Event is saved. You can select Open Event to access the event.
Use this method when you want to add multiple events with basic information, such as Unit ID, Event Start date, Capacity Event Type.
In the upper-right corner of the page, select Create Event.
The Event Creation page appears.
In the grid, enter values in the following fields:
Unit ID: Select the GAA Unit for which you want to add a Primary Event.
Start Date: Select the date for which you want to add a Primary Event.
Select
The new Primary Event is saved. You can repeat the above steps to add additional Primary Events.
Results
What's Next?
Copyright © 2018 General Electric Company. All rights reserved.