APM Event Records

APM Event records store information about the fields that are defined for the APM Event family in the baseline GE Digital APM database. This topic provides an alphabetical list and description of the fields that exist for the APM Event family and appear on the APM Event datasheet. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field Data Type Description Behavior and Usage
APM Event Date Date Indicates when the event began.

This field is populated automatically using the value in the Event Start Date field in the Primary Event record that is linked to the APM Event record.

This field is required.

APM ID Character Indicates a value that identifies the APM Event.

This field is populated automatically using the following template:

APM~<Unit Name>~<Event Start Date>

where:

  • <Unit Name> is the value in the Unit ID field in the GAA Unit record that is linked to the Primary Event record for which the APM Event record exists.
  • <Event Start Date> is the value in the Event Start Date field in the Primary Event record that is linked to the APM Event record.

The value in the Description field describes the APM event. You can enter a description into this field.

Critical Event Flag Boolean Indicates if the event was a critical event. If the value in this field is True, the event was a critical event. If the value in this field is False, the event was not a critical event.
Plant ID Character Indicates the plant in which the event occurred.

This field is populated automatically with the value in the Plant ID field in the GAA Plant that is linked to the GAA Unit that is linked to the Primary Event for which the APM Event exists.

The value in the Description field describes the name of Plant in which the event occurred. This field is populated automatically with the value in the Plant name field in the GAA Plant that is linked to the GAA Unit that is linked to the Primary Event for which the APM Event exists.

Primary Cause Character A value that indicates the cause code for the event.

This field is populated automatically with the value in the Cause Code field in the Primary Event record that is linked to the APM Event record.

The value in the Description field describes the cause code for the event. This field is populated automatically with the value in the Cause Code Description field in the Primary Event that is linked to the APM Event.

Primary Contact Character Indicates the person responsible for information about the APM event. You can enter an alphanumeric value into this field.
Unit ID Character Indicates the unit to which the event occurred.

This field is populated automatically with the value in the Unit ID field in the GAA Unit record that is linked to the Primary Event for which the APM Event exists.

This field is required.

The value in the Description field describes the name of Unit in which the event occurred. This field is populated automatically with the value in the Unit Name field in the GAA Unit that is linked to the Primary Event for which the APM Event exists.

Copyright © 2018 General Electric Company. All rights reserved.