Event Records

Event records store information about the fields that are defined for the Primary Event and Contributing Event families in the baseline GE Digital APM database. This topic provides an alphabetical list and description of the fields that exist for the Primary Event and Contributing Event families and appear on the Event datasheet. The information in the table reflects the baseline state and behavior of these fields. The values in these fields are defined by NERC in the GADS DRI and CEA in the Generation Equipment Status ERIS. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field Data Type Description Behavior and Usage
Ambiguous Date and Time Preference Character Identifies whether the date and time entered in the Event Start Date field occurred before or after the clock was reset.

This field is disabled by default. This field is enabled and required when you enter an ambiguous date and time in one of the following fields:

  • Event Start Date
  • Event End Date
  • Work Started
  • Work Ended

You can select one of following values in this field:

  • First Occurrence: Select this option if the date and time that you entered in the Event Start Date field occurred before the clock was reset.
  • Second Occurrence: Select this option if the date and time that you entered in the Event Start Date field occurred after the clock was reset.

This field exists in the Primary Event family but not the Contributing Event family.

Amplification Code Character Identifies the failure mode of the event.

This field is enabled only when the Cause Code field is populated with a value. A baseline rule exists to populate this field with a list of values from the Amplification Code field in the Amplification Codes records.

Notes: Consider the following when the Primary Event is associated with a GAA Unit in which the value in the Primary Regulatory Body field is North American Electric Reliability Corporation (NERC):

  • If you set the Capacity Event Type field to U1, the Amplification Code field can be set to 84, T1, or T2 only. If you set Amplification Code as 84, a message appears asking you to select T1 or T2 when you have a confirmed cause of event.
  • If you set the Capacity Event Type field to D1, D2, D3, D4, PD, DP, or DM, the Amplification Code field can be set to 82 or 83 only.
  • If you set the Capacity Event Type field to U1, D1, D2, D3, D4, PD, DP, or DM, the Amplification Code field becomes a mandatory field.

This field is required when the Primary Event is in the Unit Approved state.

This field is included in NERC event reports.

Capacity Event Type Character

Identifies the type of event.

For NERC,

  • For a Primary Event, this field contains a list of values defined in the GAA Event Types records.
  • For a Contributing Event, this field is disabled and populated automatically with the value in the Capacity Event Type field in the Primary Event to which it is linked.

For CEA, this field contains a list of values defined in the GAA Event Types records.

This field excludes the Event Types based on the Unit Types that you selected in the Excluded Unit Type field in the GAA Event Types record.

This field is included in NERC event reports.

This field is required.

Cause Code Character Identifies the cause code of the cause for the event.

A baseline rule exists to populate this field with a list of values in fields in Cause Codes records using the format Cause Code (Cause Code Description).

This field is required when the Primary Event is in the Unit Approved state.

Cause Code Component Character Identifies the cause code component for the cause of the event.

A baseline rule exists to populate this field with a list of values in the Component field in Cause Codes records.

This field is required when the Primary Event is in the Unit Approved state.

Cause Code Description Character Identifies the description of the cause code associated with the cause of the event.

A baseline rule exists to populate this field with a list of values in the Cause Code Description field in Cause Codes records.

This value is defined by NERC in the GADS DRI and CEA in the Generation Equipment Status ERIS.

This field is required when the Primary Event is in the Unit Approved state.

Cause Code System Character Identifies the system for the cause code associated with the event.

A baseline rule exists to populate this field with a list of values in the System field in Cause Code records.

This field is required when the Primary Event is in the Unit Approved state.

Cost Calculation Status Character Indicates the status of the cost calculation.

This field is populated automatically with information regarding the status of the calculation performed in the Capacity Incident Cost field.

This field exists in the Primary Event family but not in the Contributing Event family.

Count of Contributing Events

Character Indicates the number of Contributing Events that exist for the Primary Event.

This field is disabled and populated automatically with a value that indicates the number of Contributing Events that are linked to the Primary Event. The value in this field is updated each time you link a new Contributing Event to the Primary Event and each time you unlink a Contributing Event from the Primary Event.

This field exists in the Primary Event family but not the Contributing Event family.

Cumulative Engine Starts at Time of Event

Character

Identifies the total number of engine starts the unit had experienced at the time the event occurred.

This field is available in the Additional Reporting section for a Primary Event.

Cumulative Fired Hours at Time of Event

Character

Identifies the total cumulative number of hours the unit spent generating power at the time the event occurred.

This field is available in the Additional Reporting section for a Primary Event.

Dominant Derate Boolean

Indicates whether the Event represents a dominant derate event.

This field is enabled only when the Capacity Event Type field contains a value that identifies the event as a derate event. If the value in this field is:

  • True, the Event represents the dominant derate event.
  • False, the Event does not represent the dominant derate event.

This field exists in the Primary Event family but not in the Contributing Event family.

End Date is Estimated? Boolean

Indicates whether the value in the Event End Date field is an estimate.

Select this check box when the value in the Event End Date field represents an estimate of when the event ended or will end.

Clear this check box if the value in the Event End Date field represents the actual time that the event ended.

Note: This check box is selected automatically if you enter a future date in the Event End Date field.

This field exists in the Primary Event family but not in the Contributing Event family.

Event Contribution Code Character

Indicates how the incident contributed to the event.

A baseline rule exists to populate this field with a list of System Codes in the MI_GAA_EVENT_CONTR_CODE System Code Table.

You can change the value by selecting one of the following options:

  • 2-Contributed to Primary Cause: Indicates that the event represents a secondary cause that contributed to the primary cause of the event.
  • 3-Work done during the event: Indicates that the event represents work that was done during the event.
  • 5-After startup, delayed unit from reaching load point: Indicates that the event delayed the unit from reaching its dependable capacity after startup and prevented the unit from filling its load requirement.

This value is included in the NERC event reports.

This field exists in the Contributing Event family but not in the Primary Event family.

Event Duration Character

Indicates how long the event lasted.

This field is disabled and calculated automatically using the following formula:

Event End Date - Event Start Date

The Event Duration takes into account any existing Daylight Saving Time Reference records for the time period between the Event Start date and Event End date.

Event End Date Date

Indicates the date and time that the event ended.

This value is included in NERC event reports.

Event ID Character
  • For a Primary Event, this value identifies the event with a value that is unique to all Primary Events associated with a given GAA Unit.
  • For a Contributing Event, this value identifies the Primary Event for which the Contributing Event exists.
This field is disabled and populated automatically.
Event Number Numeric

Indicates the order in which the event occurred with respect to other events that exist for the same unit.

  • For a Primary Event, the value indicates the chronological order in which the event took place. When you create a Primary Event, this field is populated automatically. For example, when you create the third Primary Event for a given GAA Unit for a given reporting month and year, this field will be populated automatically with the value 3 (three).
  • For a Contributing Event, this field is populated automatically with the value in the Event Number field in the Primary Event to which it is linked.

This field does not appear on the datasheet.

Event Start Date Date

Indicates the date and time that the event began.

This value is included in NERC event reports.

This field is required.

Failure Mechanism Code Character

Indicates the manner in which the component failed.

A baseline rule exists to populate this field with a list of System Codes in the MI_GM_FAILURE_MECHANISM System Code Table.

This field exists in the Primary Event family but not the Contributing Event family.

This field is available in the Additional Reporting section for a Primary Event.

Gross Available Capacity Character

Identifies the gross available generation capacity of the unit during the event.

  • This field is only enabled for a Reserve Shutdown event. This field contains a value that is calculated depending on the value in the Capacity Event Type field. If the value in the Capacity Event Type field contains a value that identifies the event as:
    • A derate event, this field will become required, and the value must be less than the value in the Gross Dependable Capacity field. This field is cleared and becomes required when the Gross Derate Amount field contains no value or the value 0 (zero). If the Gross Derate Amount field contains a value other than 0 (zero), this field will be populated automatically using the following formula:

      Gross Dependable Capacity - Gross Derate Amount

    • An outage event, this field will become disabled and populated with the value 0 (zero).
  • For a Contributing Event, this field is disabled and populated automatically with the value in the Gross Available Capacity field in the Primary Event to which it is linked.
Gross Dependable Capacity Character Identifies the gross dependable generation capacity of the unit at which the event occurred.

This field is populated automatically with the value in the Gross Dependable Capacity field in the Unit Capacity record for a GAA Unit based on the start date of the Primary Event.

This field exists in the Primary Event family but not the Contributing Event family.

Gross Derate Amount Character

Indicates the gross amount of generation capacity that was lost during the event.

  • This field is only enabled for Derate events. This value is used to calculate the value in the Gross Available Capacity field. The default value is 0 (zero). If the value in the Capacity Event Type field contains a value that identifies the event as:
    • A derate event, this field will be optional. If this field contains a value other than 0 (zero), the value in the Gross Available Capacity field will be disabled and populated automatically using the following formula:

      Gross Dependable Capacity - Gross Derate Amount

      If this field contains no value or the value 0 (zero), the Gross Available Capacity field becomes required.

    • An outage event, this field will become disabled and populated with the value 0 (zero).
  • For a Contributing Event, this field is disabled and populated automatically with the value in the Gross Derate Amount field in the GAA Unit for which the Contributing Event exists.
Gross Maximum Capacity Character Identifies the gross maximum generation capacity of the unit.

This field is populated automatically with the value in the Gross Maximum Capacity field in the Unit Capacity record for a GAA Unit based on the start date of the Primary Event.

This field does not appear on the datasheet.

Man-hours Worked Numeric Identifies the number of man hours that were worked correcting the cause of the event or repairing the unit.

You can enter a value manually.

Net Available Capacity Character

Identifies the net available capacity of the unit during the event.

  • This field is only enabled for Reserve Shutdown events. This field contains a value that is calculated depending on the value contained in the Capacity Event Type field. If the value in the Capacity Event Type field contains a value that identifies the event as:
    • A derate event, this field will become required, and the value must be less than the value in the Net Dependable Capacity field. This field is cleared and becomes required when the Net Derate Amount field contains no value or the value 0 (zero). If the Net Derate Amount field contains a value, this field will be populated automatically using the following formula:

      Net Dependable Capacity - Net Derate Amount

    • An outage event, this field will become disabled and populated with the value 0 (zero).
  • For a Contributing Event, this field is disabled and populated automatically with the value in the Net Available Capacity field in the GAA Unit that contains a value in the Unit ID field that matches the value in the Unit ID field in the Event.
Net Dependable Capacity Character

Identifies the net dependable generation capacity of the unit at which the event occurred.

This field is populated automatically with the value in the Net Dependable Capacity field in the Unit Capacity record for a GAA Unit based on the start date of the Primary Event.

This field exists in the Primary Event family but not the Contributing Event family.

Net Derate Amount Character

Indicates the net amount of generation capacity that was lost during the event.

  • This field is only enabled for Derate events. This value is used to calculate the value in the Net Available Capacity field. The default value is 0 (zero). If the value in the Capacity Event Type field contains a value that identifies the event as:
    • A derate event, this field is an optional field. If this field contains a value other than 0 (zero), the value in the Net Available Capacity field will be disabled and populated automatically using the following formula:

      Net Dependable Capacity - Net Derate Amount

      If this field contains no value or the value 0 (zero), the Net Available Capacity field is cleared and becomes required.

    • An outage event, this field will become disabled and populated with the value 0 (zero).
  • For a Contributing Event, this field is disabled and populated automatically with the value in the Net Derate Amount field in the GAA Unit that contains a value in the Unit ID field that matches the value in the Unit ID field in the Event.
Net Maximum Capacity Character Identifies the net maximum generation capacity of the unit at which the event occurred.

This field is populated automatically with the value in the Net Maximum Capacity field in the Unit Capacity record for a GAA Unit based on the start date of the Primary Event.

This value is defined by NERC in the GADS DRI.

This field does not appear on the datasheet.

OMC Event Boolean

Indicates whether the event occurred for reasons that are outside of management control, such as a flood or lightning.

If the value in this field is:

  • True, the event is considered outside of management control.
  • False, the event is considered to be within management control.
Potential Capacity Incident Cost Character

Identifies the potential cost of the event.

This field is disabled and populated automatically with the calculated event cost, if a cost has been calculated.

This field exists in the Primary Event family but not in the Contributing Event family.

Primary Incident ID Character Identifies the Primary Event for which the Contributing Event exists.

This field is disabled and populated automatically with the value in the Event ID field in the Primary Event to which the Contributing Event is linked.

This field exists in the Contributing Event family but not the Primary Event family.

Problem Alert Boolean

Indicates whether the problem that caused the event is the result of a design flaw or standard operating practices.

If the value in this field is:

  • True, the problem was the result of a design flaw or standard operating practices.
  • False, the problem was the result of another cause.
Refresh Incident Cost Boolean

Indicates whether the GE Digital APM system should refresh the cost calculation for the Primary Event.

When you save the Primary Event, if the value in this field is:

  • True, the GE Digital APM system will update the value in the Capacity Incident Cost field and then save the new value, along with any other changes that you made the Primary Event.
  • False, the GE Digital APM system will save any changes that you made to the Primary Event but will not update the value in the Capacity Incident Cost field.

This field exists in the Primary Event family but not the Contributing Event family.

Reporting Month Character

Identifies the month for which the data in the Primary Event should be reported.

This field is disabled and populated automatically with the month indicated by the value in the Event Start Date field.

This field exists in the Primary Event family but not the Contributing Event family.

Reporting Year Numeric

Identifies the year for which the data in the Primary Event should be reported.

This field is disabled and populated automatically with the year indicated by the value in the Event Start Date field.

This field exists in the Primary Event family but not the Contributing Event family.

Revision Numeric

Identifies the revision number of the Event and should be incremented each time you re-submit a report which includes information in the Event to a Regulatory Organization.

By default, for an Event submitted to the regulatory organization for the first time, the value in this field is set to 0.

You must increase the value in this field each time you submit a report to the Regulatory Organization.

Start Date is Estimated? Boolean

Indicates whether the value in the Event Start Date field is an estimate.

Select this check box when the value in the Event Start Date field represents an estimate of when the event ended or will end.

Clear this check box if the value in the Event Start Date field represents the actual time that the event ended.

This field exists in the Primary Event family but not the Contributing Event family.

Trip Mechanism Character

Indicates how the unit was shut down during the event.

This field contains no value by default, and a baseline rule exists to populate this field with a list of the following values:

  • A - Automatic: The unit shut down automatically.
  • M - Manual: The unit was shut down manual by an operator.

After you select a value in this field and save the Event record, you will not be able to clear the field.

This field is available in the Additional Reporting section for a Primary Event.

Unit ID Character

Identifies the Unit ID of the GAA Unit record with which the Event is associated.

  • For a Primary Event, a baseline rule exists to populate this field with a list of values from the Unit ID and Unit Name fields in all GAA Unit records that you have permission to modify using the formula Unit ID (Unit Name).

    This field is required when the Primary Event is in the Unit Approved state.

  • For a Contributing Event, this field is disabled and populated automatically with the value in the Unit ID field in the Primary Event for which the Contributing Event exists.
Unit Name Character

Identifies the name of the unit to which the event occurred.

This field is disabled and populated automatically using values from Performance or GAA Unit records.
Validate Incident Boolean

Indicates whether the GE Digital APM system will validate the record against all other existing Primary Events.

When you save the Primary Event, if the value in this field is:

  • True, the GE Digital APM system will check all other Primary Events to validate any sequential event pairs of which the Primary Event is a part, update the value in the Incident Validation Status field if necessary, and then save the Primary Event to the database.
  • False, the GE Digital APM system will save any changes that you made to the record, but will not validate the Primary Event against any other Primary Events.

This field exists in the Primary Event family but not the Contributing Event family.

Verbal Description Character

Describes the event.

This field can be used to store any information about the event that is not captured in the other fields in the Event record.

When you create a Primary Event, you can enter a verbal description of up to 255 characters. When you generate a NERC Event Report, the verbal description in the generated report will display only the first 84 characters of the description that you entered in the Verbal Description field.

This field is required when the Primary Event is in Unit Approved state.

Work Duration Character

Indicates the duration of the work that was completed as a result of the event.

This field is disabled and populated automatically using the following formula:

Work Started + Work Ended

Work Ended Date

Indicates the date and time when work on the unit ended as a result of the event.

If you enter an ambiguous date and time in this field, a message will appear and the Ambiguous Date and Time Preference field will be enabled and required.

This value is included in NERC event reports.

Work Started Date

Indicates the date and time when work on the unit started as a result of the event.

If you enter an ambiguous date and time in this field, a message will appear and the Ambiguous Date and Time Preference field will be enabled and required.

This value is included in NERC event reports.

Copyright © 2018 General Electric Company. All rights reserved.