About UOM Conversion Set

A UOM Conversion Set is simply a group of UOM conversions. Each Security User will have a UOM Conversion Set associated with it to determine how numeric values will be converted and displayed for that user throughout the GE Digital APM systems. You can manage all the UOM Conversion Sets in your system through the UOM Conversion Set workspace, where you can add, modify, and delete UOM Conversion Sets.

UOM Conversion Sets are useful for customizing the display of numeric values for the users in your system. Any numeric field can have a UOM defined for it to indicate the unit of measure for the stored value. The base (or stored) UOM, however, may not be appropriate for all users. For instance, some users may prefer to see a value that is stored in inches converted to and displayed as centimeters. Other users might prefer to see the same value converted to millimeters. You can allow for numeric values to be converted to different display values for different users by defining UOM Conversion Sets.

To take advantage of this functionality, you will need to complete the following steps:

  1. Define the necessary base UOMs. For example, Inches.
  2. For each base UOM, define all required UOM conversions. For example, for Inches, create two UOM conversions, one for Centimeters and one for Millimeters.
  3. For each type of user, create an appropriate UOM Conversion Set. For example, we would create two UOM Conversion Sets.

  4. Associate each UOM Conversion Set with the Security User who will want to see the associated UOM conversions by using the Security Manager. For example, for any user who wants to see values stored in inches displayed in centimeters, choose Conversion Set A.

Copyright © 2018 General Electric Company. All rights reserved.