Create a UOM Conversion Set

UOM Conversion Sets are useful for customizing the display of numeric values for the users in your system. Any numeric field can have a UOM defined for it to indicate the unit of measure for the stored value. The base (or stored) UOM, however, may not be appropriate for all users. For instance, some users may prefer to see a value that is stored in inches converted to and displayed as centimeters. Other users might prefer to see the same value converted to millimeters. You can allow for numeric values to be converted to different display values for different users by defining UOM Conversion Sets.

Steps

  1. Access the UOM Conversion Set section.
  2. Select .

    The New Conversion Set window appears.

  3. In the Conversion Set ID box, enter an ID for the conversion set.
  4. In the Description box, enter a description of the conversion set.

    The description is optional. 

  5. Select OK.

    The new UOM conversion set is created and appears in the UOM Conversion Set workspace.

Copyright © 2018 General Electric Company. All rights reserved.