EAM System records are used to store information about your SAP or SAP PI Systems to facilitate data extracts and loads to and from SAP or SAP PI.
When you transfer data from GE Digital APM to your EAM system during any of the following workflows, the GE Digital APM system uses EAM System records to determine which EAM system to use:
In addition, EAM System records are used by the Equipment Characteristics Extraction Adapter and the Functional Location Characteristics Extraction Adapter in both of the following workflows:
When you create CMMS Classification Type records, EAM System records are used to determine which EAM system information to use to populate the CMMS System ID field.
When you refresh the GE Digital APM system to reflect the current SAP classifications and characteristics, EAM System records are used to determine the EAM system in which to look for the current classifications and characteristics.
This topic provides an alphabetical list and description of the fields that exist for the EAM System family. The information in the table reflects the baseline state and behavior of these fields.
This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.
In new EAM System records, you will
need to delete all angle brackets and:
Replace
the text SAP_SERVER_IP with the IP address of the SAP
Server.
Replace
the text SAP_SYSTEM_NUMBER with the SAP System number.
Replace
the text SAP_CLIENT_NUMBER with the SAP Client number.
Connection Type
Character
The type of connection that will be
used to connect to the EAM system.
This field is available on the SAP System for RCMO datasheet, and is not enabled by default.
The default and recommended value is RFC.
This connection type uses a REST web service call as an intermediary between SAP and GE Digital APM, thereby avoiding RFC calls directly between GE Digital APM and your SAP server.
Note: If necessary, you can change the connection type to RFC Direct. Changing this value will bypass APM Connect and use a direct RFC connection when connecting your GE Digital APM system and your SAP system.
To change this value, you must first enable editing on the datasheet.
Default EAM System?
Boolean
A value that indicates whether this
EAM system should be used by default when transferring data between your
GE Digital APM system and your SAP system.
On the datasheet, you can select
the check box to identify this SAP system as the Default EAM System.
Password
Character
The password to the SAP system.
The password that you enter will be encrypted
and displayed as asterisks on the datasheet.
ITS URL
Character
The URL to the ITS Server.
In new EAM System records, you will
need to delete the angle brackets and replace the text its_or_integrated_its_server_url with
the appropriate URL.
Entering this value is optional.
Name
Character
The name of the SAP system.
You can enter any name, but we
recommend that you use the format <SYSID>-<CLIENT>,
where <SYSID> is the System ID of the SAP system and
<CLIENT> is the Client number. By doing so, the value in the Name field
will match the value that will be populated automatically in the System
ID field.
System ID
Character
The ID of the SAP system.
This field is populated
automatically after you test the connection to
the SAP system using the Test Connection link on the Associated
Pages menu.
Specifically, the System ID field
is populated automatically with the name of the SAP system, using the format <SYSID>-<CLIENT>,
where <SYSID> is the System ID of the SAP system and <CLIENT> is
the Client number.
System Type
Character
EAM system type.
SAP
User ID
Character
The User ID of a user that can log
in to the SAP system.
The password that you enter will be encrypted and displayed as asterisks on the datasheet.
SAP PI AAE
Boolean
If you are using SAP 7.3 or above, you may use the Advanced Adapter Engine (AAE). This parameter allows this functionality to be used during extraction.
You must enter one of the following values:
true: If you are using AAE.
false: If you are not using AAE. This is the default.
SAP PI Host
Character
The SAP PI server host.
Enter your unique value.
SAP PI Port
Character
The SAP PI server port.
Enter your unique value.
SAP PI Receiver Party
Character
The receiver determined in the communication channel section in SAP.
This field is optional. Enter your unique value.
SAP PI Receiver Service
Character
The receiver service determined in the communication channel section in SAP.
This field is optional. Enter your unique value.
SAP PI Sender Party
Character
The receiver sender determined in the communication channel section in SAP.
This field is optional. Enter your unique value.
SAP PI Sender Service
Character
The sender service determined in the communication channel in SAP.
The default value is GE_APMConnect.
System Type
Character
EAM system type.
SAP_PI
User ID
Character
The User ID of a user that can log
in to the SAP PI system.