Technical Characteristic

Technical Characteristics records are used to store information about your SAP Technical Characteristics to facilitate data extracts and loads to and from SAP.

This topic provides an alphabetical list and description of the fields that exist for the Technical Characteristic family and appear on the baseline EAM System datasheet. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Name

Character

The name of the characteristic.

None

Value

Character

The value assigned to the characteristic.

If multiple values are assigned to a characteristic in SAP, all of those values will be displayed in the Value field, separated by commas.

Copyright © 2018 General Electric Company. All rights reserved.