CMMS Classification records are available on the baseline Classification Type Classifications master-detail datasheet, the table explains how these fields behave when you are viewing CMMS Classification records in the context of this master-detail record.
This topic provides an alphabetical list and description of the fields that exist for the CMMS Classification family. The information in the table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Class Group |
Character |
The SAP class group to which this classification belongs. |
The value in this field is set automatically, and this field is disabled. |
Classification |
Character |
The ID of the classification (as it is defined in the SAP system). |
On the datasheet, the value in this field is formatted as a hyperlink, which you can select to see all of the characteristics that belong to this classification. This field is disabled. |
Classification Description |
Character |
The description of the classification (as it is defined in the SAP system). |
This field is disabled. |
CMMS System ID |
Character |
The value in the System ID field in the EAM System record whose Name field contains the value that is stored in the CMMS System field in this record. |
This field is populated automatically and used internally by the GE Digital APM system. This field is not available on the baseline datasheets. |
Extract From CMMS System |
Boolean |
A value that identifies whether or not characteristics for this classification will be extracted from the SAP system. |
On the datasheet, you can select this check box if you want to extract characteristics belonging to this classification. |
Internal Classification Number |
Character |
This value is used internally by the GE Digital APM system. |
The value in this field is set automatically, and this field is disabled. |
Copyright © 2018 General Electric Company. All rights reserved.