CMMS Characteristic

CMMS Characteristic records are used by the SAP Adapters to facilitate data extracts and loads to and from SAP.

This topic provides an alphabetical list and description of the fields that exist for the CMMS Characteristic. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Characteristic Description

Character

The description of the characteristic (as it is defined in the SAP system).

This field is disabled.

Characteristic Name

Character

The ID of the characteristic (as it is defined in the SAP system).

On the datasheet, the value in this field is formatted as a hyperlink, which you can select to open the CMMS Characteristic by itself, outside of the context of its master CMMS Classification record.

This field is disabled.

Class Group

Character

The SAP class group to which this characteristic belongs.

The value in this field is set automatically, and this field is disabled.

Classification

Character

The classification to which this characteristic belongs.

On the datasheet, the value in this field is formatted as a hyperlink, which you can select to open the CMMS Classification record representing the classification to which this characteristic belongs.

This field is disabled.

CMMS System ID

Character

The ID of the SAP System from which this characteristic will be extracted.

This field is populated automatically and used internally by the GE Digital APM system. This field is not available on the baseline datasheets.

Extract From CMMS System

Boolean

A value that identifies whether or not this characteristic will be extracted.

On the datasheet, you can select this check box if you want to extract this characteristic.

Copyright © 2018 General Electric Company. All rights reserved.