Optimize Virtual Memory
About this task
Note: If the paging file is set to grow dynamically, your system may experience severe performance problems during runtime. To ensure optimal performance, the Initial Size and Maximum Size values for the paging file must be the same so that the paging file does not grow dynamically. For more information on creation and sizing of Windows paging files, refer to Microsoft Windows Help.
Procedure
- Access Control Panel, and then select .
- Under Performance, select .
- Under Virtual Memory, select Change.
- In the Initial size and Maximum sizefields, enter a value equal to three times your physical memory.
- Select Set, and then select OK.