To add or modify a collector instance, you can provide a JSON file with the
required details. Instead of manually creating the file, you can use the
RemoteCollectorConfigurator utility to generate a sample JSON file. You can then modify
the file as needed, and then use it to add or modify the collector instance.
Add
or modify the collector
instance using the sample JSON file that you have created.