This topic provides a list of the parameters that you must
provide when you add or modify a collector instance.Table 1. Destination: Historian
Parameter |
Description |
CollectorDestination |
The type of the configuration to specify the tags whose data you
want to collect.
- If you want to use Historian Administrator to specify the tags for data collection, enter
Historian. For information, refer
to Configure Tags.
- If you want to specify the tags using an offline tag
configuration file, do not enter a value. By default, this
file is available in the following location:
<installation folder of
Historian>\GE
Digital\<collector
name>. For information, refer to
Creating Offline Configuration XML file.
|
winUserName |
The username to connect to the machine on which Historian Administrator is installed. A value is required only if:
- You want to use Historian Administrator to specify the tags for data collection.
- Historian security groups are used.
- The mode is set to 2.
|
winPassword |
The password to connect to the machine on which Historian Administrator is installed. A value is required only if:
- You want to use Historian Administrator to specify the tags for data collection.
- Historian security groups are used.
- The mode is set to 2.
|
CollectorSystemName |
The name of the machine on which you have installed the
collectors. A value is required. |
InterfaceName |
The interface name of the collector instance. A value is required
and must be unique per destination. |
InterfaceDescription |
The description of the collector instance. |
InterfaceSubType |
The subtype of the collector. For information, refer to Collector Type and Subtype. |
Type |
The type of the collector. For information, refer to Collector Type and Subtype. A value is
required. |
DataPathDirectory |
The folder in which you want to store the collector log files. If
you do not enter a value, by default, C:\\Proficy
Historian Data is considered. |
mode |
Identifies whether creating the collector instance requires a
specific user account credentials. Enter one of the following
values:
- 1: Creates the collector instance with the credentials of
the local user.
- 2: Creates the collector instance with the credentials of a
specific user. If you choose this mode, you must enter
values for the winUserName and winPassword parameters.
|
Installation parameters for an iFIX collector to send data to Historian
{
"mode": 2,
"CollectorSystemName": "<host name>",
"InterfaceDescription": "iFIX collector for unit 1",
"DataPathDirectory": "C:\\Proficy Historian Data",
"CollectorDestination": "Historian",
"winUserName": "<host name>\\<user name>",
"winPassword": "<password>",
"InterfaceSubType": "",
"DestinationHistorianUserName": "<user name>",
"DestinationHistorianPassword": "<password>",
"DestinationHistorian": "<host name>",
"General1": "",
"General2": "",
"General3": "FIX",
"General4": "",
"General5": "",
"Type": 1,
"InterfaceName": "collector_unique_name"
}
Table 2. Destination: Predix TimeSeries
Parameter |
Description |
ClientID |
The collector when interacting with Predix Time Series. This is
equivalent to the username in many authentication schemes. The
client must exist in the UAA instance identified by the identity
issuer, and the system requires that the timeseries.zones.
{ZoneId}.ingest and
timeseries.zones.{ZoneId}.query authorities are
granted access to the client for the Predix Zone ID specified. Your
Predix Time Series administrator can provide this
information. |
ClientSecret |
The secret to authenticate the collector. This is equivalent to
the password in many authentication schemes. |
CloudDestinationAddress |
The URL of a data streaming endpoint exposed by the Predix Time
Series instance to which you want to send data. Typically, it starts
with “wss://”. This value is used as part of the interface name and
default tag prefix of the collector. Your Predix Time Series
administrator can provide this URL. |
CollectorDestination |
The type of the cloud destination. For Predix TimeSeries, enter
Predix. |
CollectorSystemName |
The name of the machine on which you have installed the
collectors. A value is required. |
DataPathDirectory |
The folder in which you want to store the collector log files. If
you do not enter a value, by default, C:\\Proficy
Historian Data is considered. |
DatapointAttribute<number> |
The attributes for each data point whose values you want the
collector to collect. You can specify maximum five
attributes. |
IdentityIssuer |
The URL of an authentication endpoint for the collector to
authenticate itself and acquire necessary credentials to stream to
the Predix Time Series. In other words, this is the issuer ID of the
UAA instance that you want to use to connect to Predix Time Series.
Typically, it starts with https:// and ends with “/oauth/token”.
|
InterfaceName |
The interface name of the collector instance. A value is required
and must be unique per destination. |
InterfaceDescription |
The description of the collector instance. |
InterfaceSubType |
The subtype of the collector. For information, refer to Collector Type and Subtype. |
Proxy |
Identifies the URL of the proxy server to be used for both the
authentication process and for sending data. If the collector is
running on a network where proxy servers are used to access web
resources outside of the network, then you must provide the proxy
server settings. However, it does not affect the proxy server used
by Windows when establishing secure connections. As a result, you
must still configure the proxy settings for the Windows user account
under which the collector service runs. |
ProxyUserName |
The username to connect to the proxy server. |
ProxyPassword |
The password to connect to the proxy server. |
Type |
The type of the collector. For information, refer to Collector Type and Subtype. A value is
required. |
ZoneID |
Unique identifier of the instance to which the collector will
send data. |
winUserName |
The username to connect to the machine on which Historian Administrator is installed. A value is required only if:
- You want to use Historian Administrator to specify the tags for data collection.
- Historian security groups are used.
- The mode is set to 2.
|
winPassword |
The password to connect to the machine on which Historian Administrator is installed. A value is required only if:
- You want to use Historian Administrator to specify the tags for data collection.
- Historian security groups are used.
- The mode is set to 2.
|
mode |
Identifies whether creating the collector instance requires a
specific user account credentials. Enter one of the following
values:
- 1: Creates the collector instance with the credentials of
the local user.
- 2: Creates the collector instance with the credentials of a
specific user. If you choose this mode, you must enter
values for the winUserName and winPassword parameters.
|
Installation parameters for an iFIX collector to send data to Predix
TimeSeries
{
"ClientID": "HistQA",
"ClientSecret": "1234",
"CloudDestinationAddress": "wss://abcd.run.123.predix.io/v1/stream/messages",
"CollectorDestination": "Predix",
"CollectorSystemName": "<host name>",
"DataPathDirectory": "C:\\Proficy Historian Data",
"DatapointAttribute1": "attribute1",
"DatapointAttribute2": "",
"DatapointAttribute3": "",
"DatapointAttribute4": "",
"DatapointAttribute5": "",
"DestinationHistorian": "<host name>",
"General1": "",
"General2": "",
"General3": "abc",
"General4": "",
"General5": "",
"IdentityIssuer": "https://1234567.predix-uaa.run.aws-usw02-pr.ice.predix.io/oauth/token",
"InterfaceDescription": "1234",
"InterfaceName": "123",
"InterfaceSubType": "",
"Proxy": "http://<host name>:<port number>",
"ProxyPassword": "",
"ProxyUserName": "",
"Type": 1,
"ZoneID": "123-456-789de-rft",
"winPassword": "",
"winUserName": "",
"mode": 1
}
Table 3. Destination: MQTT
|
|
ClientID |
The name of the MQTT client. A value is required and must be
unique for an MQTT broker. |
CollectorDestination |
The type of the cloud destination. For MQTT, enter
MQTT. |
CollectorSystemName |
The name of the machine on which you have installed the
collectors. A value is required. |
DataPathDirectory |
The folder in which you want to store the collector log files. If
you do not enter a value, by default, C:\\Proficy
Historian Data is considered. |
DeviceSharedKey |
The device shared key of the MQTT broker. |
HostAddress |
The host name of the MQTT broker to which you want the collector
to send data. A value is required. |
HostPort |
The port number to connect to the MQTT broker to which you want
the collector to send data. |
InterfaceName |
The interface name of the collector instance. A value is required
and must be unique per destination. |
InterfaceDescription |
The description of the collector instance. |
InterfaceSubType |
The subtype of the collector. For information, refer to Collector Type and Subtype. |
MQTTAutoRefresh |
Indicates that the password is automatically generated on expiry;
you are not required to provide the password. |
MQTTCloudSubtype |
The subtype of the MQTT broker. |
MQTTUserName |
Enter the username to connct to the MQTT broker. |
MQTTPassword |
Enter the password to connect to the MQTT broker. |
Topic |
The MQTT topic to which you want the collector to publish
data. |
Type |
The type of the collector. For information, refer to Collector Type and Subtype. A value is
required. |
winUserName |
The username to connect to the machine on which Historian Administrator is installed. A value is required only if:
- You want to use Historian Administrator to specify the tags for data collection.
- Historian security groups are used.
- The mode is set to 2.
|
winPassword |
The password to connect to the machine on which Historian Administrator is installed. A value is required only if:
- You want to use Historian Administrator to specify the tags for data collection.
- Historian security groups are used.
- The mode is set to 2.
|
mode |
Identifies whether creating the collector instance requires a
specific user account credentials. Enter one of the following
values:
- 1: Creates the collector instance with the credentials of
the local user.
- 2: Creates the collector instance with the credentials of a
specific user. If you choose this mode, you must enter
values for the winUserName and winPassword parameters.
|
Installation parameters for an iFIX collector to send data to Google
Cloud
{
"InterfaceName": "<unique collector name>",
"InterfaceDescription": "collector for unit 3",
"Type": 1,
"mode": 2,
"CollectorSystemName": "<host name>",
"DataPathDirectory": "C:\\Proficy Historian Data",
"CollectorDestination": "MQTT",
"HostAddress": "mqtt.googleapis.com",
"HostPort": "8883",
"ClientID": "projects/mygcpproject/locations/asia-east1/registries/testmqttgcpiot/devices/testdevice",
"Topic": "/devices/gcptesting/events",
"DeviceSharedKey": "",
"MQTTCloudSubtype": "GOOGLE",
"MQTTUserName": "testusername",
"MQTTPassword": "testGoogleConnectiionstringPassword",
"MQTTAutoRefresh": "NO",
"MQTTCAFile": "",
"MQTTCertificateFile": "",
"MQTTPrivateKeyFile": "",
"MQTTPublicKeyFile": "",
"winUserName": "<host name>\\Admin",
"winPassword": "<password>",
"InterfaceSubType": "",
"DestinationHistorianUserName": "<Windows user name of the destination>",
"DestinationHistorianPassword": "<Windows password of the destination>",
"DestinationHistorian": "<host name>",
"General1": "",
"General2": "",
"General3": "FIX",
"General4": "",
"General5": ""
}
Table 4. Destination: Azure IoT Hub
|
|
CollectorDestination |
The type of the cloud destination. For Azure IoT Huv, enter
Azure. |
CollectorSystemName |
The name of the machine on which you have installed the
collectors. A value is required. |
DataPathDirectory |
The folder in which you want to store the collector log files. If
you do not enter a value, by default, C:\\Proficy
Historian Data is considered. |
DeviceConnectionString |
Identifies the Azure IoT device to which you want to send data.
Enter a value in the following format:
HostName=<value>;DeviceId=<value>;SharedAccessKey=<value> |
DeviceId |
The ID of the Azure IoT device. |
SharedAccessKey |
The shared access key of the device. |
InterfaceName |
The interface name of the collector instance. A value is required
and must be unique per destination. |
InterfaceDescription |
The description of the interface. |
InterfaceSubType |
The subtype of the collector. For information, refer to Collector Type and Subtype. |
Proxy |
Identifies the URL of the proxy server to be used for both the
authentication process and for sending data. If the collector is
running on a network where proxy servers are used to access web
resources outside of the network, then you must provide the proxy
server settings. However, it does not affect the proxy server used
by Windows when establishing secure connections. As a result, you
must still configure the proxy settings for the Windows user account
under which the collector service runs. |
ProxyUserName |
The username to connect to the proxy server. |
ProxyPassword |
The password to connect to the proxy server. |
TrasportProtocol |
The protocol that you want to use to send data to Azure IoT Hub. Enter one of the following values:
- HTTP
- MQTT
- AMQP
- MQTT_OVER_WEBSOCKETS
- AMQP_OVER_WEBSOCKETS
For information on which protocol to use, refer to Protocols and Port Numbers. |
Type |
The type of the collector. For information, refer to Collector Type and Subtype. A value is
required. |
winUserName |
The username to connect to the machine on which Historian Administrator is installed. A value is required only if:
- You want to use Historian Administrator to specify the tags for data collection.
- Historian security groups are used.
- The mode is set to 2.
|
winPassword |
The password to connect to the machine on which Historian Administrator is installed. A value is required only if:
- You want to use Historian Administrator to specify the tags for data collection.
- Historian security groups are used.
- The mode is set to 2.
|
mode |
Identifies whether creating the collector instance requires a
specific user account credentials. Enter one of the following
values:
- 1: Creates the collector instance with the credentials of
the local user.
- 2: Creates the collector instance with the credentials of a
specific user. If you choose this mode, you must enter
values for the winUserName and winPassword parameters.
|
Installation parameters for an iFIX collector to send data to Azure IoT
Hub
{
"InterfaceName": "collector_unique_name",
"InterfaceDescription": "iFIX collector for unit 2",
"Type": 1,
"mode": 2,
"CollectorSystemName": "<host name>",
"DataPathDirectory": "C:\\Proficy Historian Data",
"CollectorDestination": "Azure",
"DeviceConnectionString": "HostName=abc.azure-devices.net;DeviceId=Device1;SharedAccessKey=xxxxxxxxxx",
"TransportProtocol": "AMQP_OVER_WEBSOCKETS",
"Proxy": "<host name>:<port number>",
"ProxyUserName": "",
"ProxyPassword": "",
"winUserName": "<host name>\\<user name>",
"winPassword": "<password>",
"InterfaceSubType": "",
"DestinationHistorianUserName": "<user name>",
"DestinationHistorianPassword": "<password>",
"DestinationHistorian": "<host name>",
"General1": "",
"General2": "",
"General3": "FIX",
"General4": "",
"General5": ""
}