Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Tracer Class / WriteLine Method / WriteLine(Object,TraceLevel) Method
A value to write.
A trace level.


In This Topic
    WriteLine(Object,TraceLevel) Method
    In This Topic
    Write a message value to System.Diagnostics.Trace depending on supplied trace level.
    Syntax
    Public Overloads Shared Sub WriteLine( _
       ByVal value As System.Object, _
       Optional ByVal level As System.Diagnostics.TraceLevel _
    ) 
    public static void WriteLine( 
       System.object value,
       System.Diagnostics.TraceLevel level
    )
    public:
    static void WriteLine( 
       System.Object^ value,
       System.Diagnostics.TraceLevel level
    ) 

    Parameters

    value
    A value to write.
    level
    A trace level.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also