Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ICollectors Interface / HierarchicalBrowse Method
A collector name.
Browse position.
Node filter string.


HierarchicalBrowse Method
Initiate a hierarchical tag browse in a collector via a Historian server.
Syntax
Sub HierarchicalBrowse( _
   ByVal collectorname As System.String, _
   ByVal position As System.String, _
   ByVal nodeFiler As System.String _
) 

Parameters

collectorname
A collector name.
position
Browse position.
nodeFiler
Node filter string.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also