Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IAlarms Interface / Query Method
Contains the query criteria and fields, and other properties.


In This Topic
    Query Method (IAlarms)
    In This Topic
    Query for Alarm,Events, Alrm history etc on the Historian servers from the Alarms and Events database.
    Syntax

    Parameters

    recordsetInfo
    Contains the query criteria and fields, and other properties.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also