Before you begin
Install one of the following 32-bit or 64-bit Microsoft® Excel® applications:
- Microsoft® Excel® 2019
- Microsoft® Excel® 2016
- Microsoft® Excel® 2013
- Microsoft® Excel® 2010
About this task
You can install Excel Add-In separately or during Client Tools installation. This topic describes how to install Excel Add-In separately. However, do not install Excel Add-In on the machine on which you have installed Historian Administrator or data archiver. Procedure
-
Run the Historian installer.
-
Select Historian Excel Add-in.
The installer runs through the installation steps.
Note: If using certain versions of Windows (like Windows 10 or Windows 2019), you may receive an error message, stating that some of the DLL files are not registered. You can ignore these messages.
-
If prompted to restart your system, select Yes.
Results
Excel Add-In is installed.