Simulation Data Collector
The Simulation Collector generates random numbers and string patterns for demonstration purposes. It contains a user-defined number of tags. You can configure the number of tags in the Collector Maintenance screen of the Historian Administrator or during installation.
The Simulation Collector generates random scaled values between 0 and 32,767. It uses the Engineering Units Hi
and Lo
values configured for each tag to scale the 0 to 32,767 pre-set values into appropriate engineering units. The default is 0 to 200,000.
The Simulation Collector also provides five string-simulation tags that generate random alphanumeric data. The Simulation Collector supports browsing and can automatically add tags in the same manner as the iFIX and OPC Collectors through the Add Tags from Collector dialog box.
Note: You can create more simulation string tags by manually adding string tags with the
CollectorName.Simulation.StringXXXX
naming convention to the Simulation Collector.Summary of Simulation Collector Features
Feature | Capability |
---|---|
Browse Source For Tags | Yes |
Browse Source For Tag Attributes | Yes |
Polled Collection | Yes |
Minimum Poll Interval | 100 ms |
Unsolicited Collection | No |
Timestamp Resolution | 1 ms |
Accept Device Timestamps | No |
Floating Point Data | Yes |
Integer Data | Yes |
String Data | Yes |
Binary Data | No |
Python Expression Tags | Yes |