Configuration tab for Simulation Collectors

About this task

To display the Configuration tab for a Simulation Collector:

Procedure

  1. Select a Simulation Collector from the list on the left and click the Configuration tab.
  2. The Number of Tags field displays the number of tags currently added to the Simulation Collector. Edit the Number of Tags field to increase or decrease the number of Simulation tags available for addition to the Historian system.


  3. The Function Period field configures the period, in seconds, of the SIN,STEP, and RAMP functions implemented in the Simulation Collector.
    The default is 60 seconds.