Installing Alarms and Events
About this task
Selecting the Install Alarms and Events option in the Install Historian screen installs the Historian Alarm Archiver. You must specify the SQL Server database details for the archiver, as the archiver requires access to SQL Server.
Important:
- If you have the Alarms and Events component installed on a pre-7.0 version of Historian, then after you upgrade to Historian Server 7.0, you must install the Alarms and Events component separately.
- The Alarms and Events component must be installed on the same machine as the Data Archiver.
- When upgrading from 4.5 to 7.0 Alarms and Events, since the DB Schema for 4.5 is different, if you select the same database name that is pre-populated by default, you will get an error message:
Later or Higher version of Alarms and Events database is already installed. Hence, you cannot proceed further.
You need to enter a different database name and then proceed with the upgrade.
To install Alarms and Events: