Command-Line Syntax

Command

Collectors_Install.exe

Argument

-s, -silent

Using either of these flags directs the install to progress silently, with no user interaction.

Parameters

  • <CollectorName>_AddLocal (1=install and 0= uninstall)
  • <CollectorName>_sourceservername
  • <CollectorName>_destinationservername
    Note: destinationservername and cloud parameters do not apply to the File Collector, iFIX Collector, or Calculation Collector.

    For a Historian destination, use the machine name. For a Predix Cloud destination, use "Cloud".

  • <CollectorName>_clientsecret
  • <CollectorName>_clouddestaddress
  • <CollectorName>_clouddestaddress
  • <CollectorName>_configserver
    Note: If using offline configuration, set this parameter equal to none. For example:
    HistorianS2SCollector_configserver=none
  • <CollectorName>_identityissuer
  • <CollectorName>_clientid
  • <CollectorName>_zoneid
  • <CollectorName>_proxy
  • <CollectorName>_proxyusername
  • <CollectorName>_proxypassword
  • <CollectorName>_datapointattributekey1
  • <CollectorName>_datapointattributevalue1
  • <CollectorName>_datapointattributekey2
  • <CollectorName>_datapointattributevalue2
  • <CollectorName>_datapointattributekey3
  • <CollectorName>_datapointattributevalue3
  • <CollectorName>_datapointattributekey4
  • <CollectorName>_datapointattributevalue4
  • <CollectorName>_datapointattributekey5
  • <CollectorName>_datapointattributevalue5