Stop an Application on Predix Edge

About this task

You can stop an application if you want to modify the configuration for the application. For example, if you want to modify the properties of tags used by the server-to-server collector, you must first stop the application, modify the properties, and then run the application.

Procedure

  1. Access Predix Edge Technician Console (PETC).
  2. In the DEPLOYED INSTANCES section, select the check box corresponding to the application that you want to stop.
  3. Select Action > Stop.
    The application is stopped.