Overview of the OPCUA DA Collector
The OPCUA DA collector collects data from any OPCUA-compliant OPCUA DA server, and sends it to the Historian database. The collector automatically determines the capability of the OPCUA server to which it is connected. For more information on the capabilities of the collector, refer to Capabilities of the OPCUA DA Collector.
You can set up the OPCUA DA collector on Predix Edge or a generic Linux distribution such as Ubuntu or CentOS.