Environment Variables Used by the REST Query
The environment variables used by the REST query are available in the rest-query-config file. The following table describes these variables.
Note: For a secure connection, add - zones.<zone-id>.query, historian_rest_query_service.user in the UAA scopes and authorities.
Environment Variable | Description | Default Value | Valid Values |
---|---|---|---|
HISTORIAN_HOSTNAME | The IP address of the Historian database. | ||
HISTORIAN_MAX_DATA_QUERY | The maximum number of data points to be retrieved for one tag from the Historian database. | 10000 | As many tags as you have in the Historian archiver. |
HISTORIAN_MAX_TAG_QUERY | The maximum number of tags retrieved from the Historian database. | 5000 | |
DISABLE_REST_QUERY_SECURITY | Indicates whether security must be enabled. | true |
|
ZAC_UAA_CLIENTID | Client ID of OAUTH2 server. A value is required if the DISABLE_REST_QUERY_SECURITY variable is set to false. | ||
ZAC_UAA_CLIENT_SECRET | Client secret of the OAUTH2 server. A value is required if the DISABLE_REST_QUERY_SECURITY variable is set to false. | ||
ZAC_UAA_ENDPOINT | URL of OAUTH2 server. A value is required if the DISABLE_REST_QUERY_SECURITY variable is set to false. | ||
USE_PROXY | Indicates whether a firewall is present between the OAUTH2 server and the REST query. | true |
|
PROXYURL | The URL of the proxy server (along with the port number). |