Create an Archive Automatically
About this task
You can allocate maximum 256 GB for an archive.
Procedure
- Access Historian Administrator.
-
Select DataStores.
-
Select Data Store Options.
-
Enter values as described in the following table.
Field Description Automatically Create Archives Select Enabled. Overwrite Old Archives Specify whether you want to overwrite old archives with new ones. Exercise caution in enabling this option. We recommend that you backup archives if you want to enable this option. Default Size Enter the size of the current archive after which you want to create a new archive. This field is available only if you have selected By Size in the adjacent drop-down list box. If, however, you want to create archives after a duration, select Days or Hours, and then enter the value in the Archive Duration field.
Archive Duration Enter the duration after which you want to create a new archive. This field is available only if you select Days or Hours in the adjacent drop-down list box. If, however, you want to create an archive when the current one reaches a particular size, select By Size, and then enter the value in the Default Size field.
Default Archive Path Enter the path to the folder in which you want to store the archive files. Default Backup Path Enter the path to the folder in which you want to store the backup files. Base Archive Name Enter the base name for the archive. This name will be appended with a number to identify the sequence of the archive. Free Space Required Enter the free space that is required to create the archives. Store OPC Quality Specify whether you want to store OPC quality in the archive. Use Caching Specify whether you want to use caching in the archive. Data is Read-Only After (Hours) Specify the duration, in hours, after which you want to archive to be read-only. Generate Message on Data Update Specify whether you want to generate a message when data is updated in the archive. -
Select Update.
Archives will be created automatically when the current one reaches the size (or after the duration) that you have specified.