Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IPublish Interface / SetDestinationServer Method
Name of target collector, typically an instance of ServerToServer Distributor.
A Historian server name (or IP).


In This Topic
    SetDestinationServer Method
    In This Topic
    Apply the given destination Historian server name to a collector.
    Syntax
    Sub SetDestinationServer( _
       ByVal collectorname As System.String, _
       ByVal destinationServer As System.String _
    ) 
    void SetDestinationServer( 
       System.string collectorname,
       System.string destinationServer
    )
    void SetDestinationServer( 
       System.String^ collectorname,
       System.String^ destinationServer
    ) 

    Parameters

    collectorname
    Name of target collector, typically an instance of ServerToServer Distributor.
    destinationServer
    A Historian server name (or IP).
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also