Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / PublishGetDestinationServerHandler Delegate
Overall operation status.
Name of the configured destination server.


In This Topic
    PublishGetDestinationServerHandler Delegate
    In This Topic
    A delegate invoked for responses to retrieving the destination server name for publishing.
    Syntax
    Public Delegate Sub PublishGetDestinationServerHandler( _
       ByVal status As Status, _
       ByVal destinationServer As System.String _
    ) 
    public delegate void PublishGetDestinationServerHandler( 
       Status status,
       System.string destinationServer
    )
    public delegate void PublishGetDestinationServerHandler( 
       Status status,
       System.String^ destinationServer
    )

    Parameters

    status
    Overall operation status.
    destinationServer
    Name of the configured destination server.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also