Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmAttribute Class
Members


In This Topic
    AlarmAttribute Class
    In This Topic
    Represents details of the Alarm Attributes Object, these are the Vendor Attributes.
    Syntax
    Public Class AlarmAttribute 
    public class AlarmAttribute 
    public ref class AlarmAttribute 
    Inheritance Hierarchy

    System.Object
       Proficy.Historian.ClientAccess.API.AlarmAttribute

    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also