Public Enum HistorianOption Inherits System.Enum
public enum HistorianOption : System.Enum
public enum class HistorianOption : public System.Enum
Public Enum HistorianOption Inherits System.Enum
public enum HistorianOption : System.Enum
public enum class HistorianOption : public System.Enum
Member | Description |
---|---|
ArchiveActiveHours | The maximum age of data samples (in hours) that can be accepted by the server. |
ArchiveAutomaticFreeSpaceHardLimit | This is hardlimit for the ihArchiveAutomaticFreeSpace option. Once this is set we wait till this hardlimit is reached instead of ihArchiveAutomaticFreeSpace |
ArchiveBackupNumArchivesToBackup | The default number of archives backed up by stand-alone ihArchiveBackup tool. |
ArchiveDataBucketSize | The size of individual archive file segments used to store data expressed in bytes. Valid values: 400 - 1400. |
ArchiveDefaultPath | The default location of archive files. |
ArchiveDefaultSize | The default size of newly created archives, expressed in MB. |
ArchiveDuration | Number of Units of time an archive can hold. Defined by ArchiveDurationType |
ArchiveDurationType | The type of archive duration. It is the integer value of ArchiveDurationType |
ArchiveIndexCountSize | The number of child index nodes to use within archive files. Valid values: 2 - 5. |
ArchiverAllowFutureDataWrites | |
ArchiverAutoDeleteArchives | if 0 don't let the data archiver delete archives in low disk space |
ArchiverBackupType | |
ArchiverMaxConfigAgeToAvoidWaitingForConfig | |
ArchiverMaxDelayWaitingForConfig | |
ArchiverMultiADSISyncInterval | |
ArchiverObsolete2 | Obsolete if 4.7. Never released to customers. Safe to reuse this in 4.7. |
ArchiverRepeatingValueStorageOptimization | When on, multi-field tags will reduce storage space by not store repeated field values, instead they only indicate that the value is the same as the previous field value. |
ArchiverReserved | |
ArchiverTcpPort | Obsolete. Now done in the registry. |
ArchiverUseStaleTagsIndex | |
ArchiveSizeIncrement | Deprecated. |
ArchiveStalePeriod | Designates the end of defined options. |
ArchiveStalePeriodCheck | |
ArchiveTotalDuration | Number of Hours that the archives for a DataStore can span (Only meaningful for scada buffer DataStores) |
ArchiveUseCaching | Whether to use caching for a specific data store - applies only to Historical Data Store |
AutoCreateArchives | Whether the server automatically creates new archives when existing archives become full. Valid values: 0 (false) or 1 (true). |
ClientStatFeature | |
CollectorIdleTime | Collector Idle time - This is the grace period in seconds . when the present time minus the maximum collector data time is greater than this grace period we add a Bad DQ . This option will only be considered for the query modifiers onlyifconnected and onlyifuptodate. |
CollectorStatusOutputs | |
ConfigurationSystemName | This is a global option which returns the system name of the CFM for use by the webservice |
DefaultArchiveBackupPath | The default location for archive file backups. |
DefaultBaseArchiveFilename | The default file name prefix of newly created archives. |
DefaultBaseArchiveName | The default name prefix of newly created archives. |
FreeSpaceRequiredForAutoArchives | The amount of free disk space required to allow automatic creation of new archives, expressed in MB. |
ihArchiverFlushInterval | if 0 do not execute flush else pick value between 10 - (60 * 60 * 24) seconds |
ihArchiverFlushType | normal or incremental |
ihArchiverHeartBeatInterval | This is the time interval that is used for the HB's |
ihArchiveUsePreparedArchive | |
ihCompressTransferChunk | whether the chunk data tranferred is compressed for GetNextChunk message. |
ihZipArchiveToTransfer | whether replicate/resync job will backup archive file as a zip file for transferring ( 0 : No, Non-Zero: Yes, Default is non-zero value ) |
Max | |
MessageOnDataUpdate | Whether to generate audit messages whenever previously recorded data is updated. Valid values: 0 (false) or 1 (true). |
OverwriteOldArchives | Whether to re-use and overwrite the oldest archive when all archives becomes full. Valid values: 0 (false) or 1 (true). |
SecurityAllowAnonymousClients | Whether to permit anonymous client connections to the server. Valid values: 0 (false) or 1 (true). |
SecurityAnonymousUsername | A name of a local user on the server that anonymous clients get mapped to for purposes of authorization. |
SecurityDomain | Internal. |
SecurityGroupsNodeName | Internal. |
SecurityStrictClientAuthentication | Whether to enforce strict client authentication - setting to 1 (true) will disallow connections from clients older than version 4.7. |
SecurityStrictCollectorAuthentication | Whether to enforce strict collector authentication - setting to 1 (true) will disallow connections from collectors older than version 4.7. |
SecurityUseClientLoginUser | Deprecated, user credentials are always validated server side. Whether to accept client validation of user credentials. Set to 0 (false) to validate user credentials on the server. Valid values: 0 (false) or 1 (true). |
SecurityUseLocalGroups | Whether to use local security groups, 1 (true), or domain security groups, 0 (false), for user authorization. Valid values: 0 (false) or 1 (true). |
ServerAllowConcurrentClientWork | Whether messages from a client can be processed concurrently, potentially out of received order. |
ServerAllowDataOverwrites | Whether the server permits replacing the value of previously recorded data samples. Valid values: 0 (false) or 1 (true). |
ServerAllowMessageThrottling | Whether to throttle incoming messages from clients to prevent disk buffering. |
ServerAuditMessage | The audit message used for electronic signatures. An empty string will use the system default message. |
ServerAuditStatus | Whether point verification is enabled. This requires the ElectronicSignatures licensed feature. Valid values: 0 (false) or 1 (true). |
ServerCacheSize | The upper memory usage target for the server, expressed in MB. |
ServerCreateOfflineArchives | Whether the server automatically creates archives for non-current data (older than the oldest archive). Valid values: 0 (false) or 1 (true). |
ServerDemoMode | Indicates whether the server is running without a license key in demo mode (read-only). Valid values: 0 (false) or 1 (true). |
ServerEquipmentDelimiter | A single character delimiting an optional equipment identifier at the beginning of tag names. |
ServerMaintainAutoRecoveryFiles | Whether to perform hourly, automated backups of the current archive and configuration. Valid values: 0 (false) or 1 (true). |
ServerMaximumMemoryBufferSize | The amount of memory the server allocates for incoming message queues, expressed in MB. |
ServerMaxIntervalRetrievalCount | The maximum number of results the server will return for any single query. Queries with more results return an error. |
ServerMaxQueryTimeSeconds | The maximum number of seconds the server will expend on any single query. Queries that take longer are terminated and return an error. |
ServerMemoryLoad | The percent of available memory currently consumed by the server (read-only). |
ServerMinimumDiskFreeBufferSize | The amount of free disk space to retain when the server expands queue files, expressed in MB. |
ServerNumCollectorWriteThreads | Deprecated, see ServerNumWriteThreads. The number of server worker threads servicing collector data write requests. Requires server restart to update. |
ServerNumDataWriteThreads | Deprecated, see ServerNumWriteThreads. The number of server worker threads servicing data write requests. Requires server restart to update. |
ServerNumFastReadThreads | Deprecated, see ServerNumReadThreads. The number of server worker threads servicing fast read requests (default: 4). Requires server restart to update. |
ServerNumGenericWriteThreads | Deprecated, see ServerNumWriteThreads. The number of server worker threads servicing generic write requests. Requires server restart to update. |
ServerNumReadThreads | The number of server worker threads servicing read requests. Requires server restart to update. |
ServerNumWriteThreads | The number of server worker threads servicing write requests (default: 1). Requires server restart to update. |
ServerOptimizeForRemoteCollectors | Deprecated. |
ServerRunningInCluster | Indicates whether the server is running managed by Microsoft Failover Clustering (read-only). Valid values: 0 (false) or 1 (true). |
ServerStoreUserQualityStatus | Whether to record custom, user-defined quality status information with data samples. Valid values: 0 (false) or 1 (true). |
ServerTargetPrivateBytes | The nominal memory usage target for the server, expressed in MB. |
ServerWorkerThreadsEnabled | Deprecated - always 1 (true). |
TagBrowseStructElements | You can set this option to just browse all the tags or browse the fields as tags for for custom data types. |
Undefined | Undefined option. |
System.Object
System.ValueType
System.Enum
Proficy.Historian.ClientAccess.API.HistorianOption
Target Platforms: Windows 98, Windows NT 4.0, Windows Millennium Edition, Windows XP Home Edition, Windows XP Professional, Windows Server 2003 family, Windows Vista, Windows Server 2008 family