Certificates
To use certificate authentication, the
user_cert_path
, user_private_key_path
and user_cert_password
fields need to be active in the options
object of your configuration, or the client_cert_path
and client_private_key_path
fields need to be in that object."options":{
"user_cert_path": "/config/client.der",
"user_private_key_path":"/config/client.key",
"user_cert_password":"<your password>"
}
Note:
The
user_cert_password
is the password used when you created your authentication certificate.To generate an authentication certificate using a Windows machine:
- Download OpenSSL for your Windows device (32-bit or 64-bit).
- Navigate to where you downloaded OpenSSL and install using the executable.
- From the folder you want to generate your authentication certificate, open a command prompt and run:
> set RANDFILE=C:\<your folder structure>\.rnd > set OPENSSL_CONF=C:\OpenSSL-Win64\bin\openssl.cfg > C:\OpenSSL-Win64\bin\openssl.exe
- You should now be at an OpenSSL> prompt, where you should run:
req -newkey rsa:2048 -days 3650 -keyout client.key -x509 -outform DER -out client.der
To generate an authentication certificate on a Unix-like system, use the following command.
openssl req -newkey rsa:2048 -days 3650 -keyout client.key -x509 -outform DER -out client.der
Note:
If you are running a simulator, be sure to copy these authentication certificates to your OPC-UA simulator.