Configuration Properties for MQTT Protocol Adapter
The following are the configuration properties for the blocks named
mqtt_source
and mqtt_sink
in the configuration below which have the types cdpin
and cdpout
respectively. Read the Generic CDP Blocks section of the Protocol Adapters documentation page for more information on these blocks and the fields within them.Property | Type | Required | Default Value |
---|---|---|---|
transport_addr | String | yes | mqtt-tcp://predix-edge-broker |
node_ref | String | yes | |
method | String | yes | pub |
log_name | String | no | |
log_level | String | no | |
options | Object | no |