Mapping the Blocks
The mappings
section is used to connect the blocks that were initialized in the blocks section.
If a block name referenced in this section does not exist in the blocks section, the protocol translator will log an error and ignore the mapping. By default, most blocks have an implicit input
and output
port that can be connected to a port from a different block so that data flows between the blocks.
In the example below, two blocks are mapped together. The output
port of the block named block1
is connected to the input
port of the block named block2
. Therefore, data will flow from block1
to block2
.
{
"blocks": {
...
},
"mappings": {
"block1:output":"block2:input",
...
}
}