Edge Core
The Edge Core is a common command execution framework that allows the abstraction of the command execution from Predix Edge Manager and the Edge Core API to execute the same commands.
The Edge Core provides a REST API that the Predix Edge Technician Console can use to dispatch commands to be issued locally. Initially, using Edge Manager on the cloud and using the technician console are mutually exclusive. A future enhancement will resolve any discrepancies between the edge device and Edge Manager.