Edge Agent Gateway and Dispatcher
The HTTP Gateway provides connectivity and authentication management between the edge device and
Edge Manager in the cloud. The HTTP Gateway performs the following tasks:
- Initiates conversation with Edge Manager on a scheduled basis.
- Receives information about the current state of the device as part of the initial connection.
- Ensures the connection is authorized and the “authentication token” is valid prior to any communication.
- Dispatches commands to appropriate command handlers.
- Responds with the status of the command execution.