Product Details and Actions under Node Manager
Within the Node Manager-Administration panel of the Configuration Hub, you can centrally control and manage the installed Proficy product(s) on the node machine. This facilitates easy registration and unregistration, as well as handling certificate requirements.
Procedure
- Log into Configuration Hub with Proficy Authentication credentials.
The NAVIGATION panel appears.
- In the NAVIGATION panel, select
Administration.
The Node Manager and License Server panels appear.
- Select Node Manager.
The Node Manager-Administration panel appears, displaying the Configuration Hub, Proficy Authentication product details, and the Node Manager row.
- Select
of the Node Manager row in the Node Manager-Administration panel.
The list of Proficy product(s) installed on the node appears. Select the product row as required, the DETAILS panel display the product details. You can perform the following actions:- PLUG-IN: Select
of the PLUG-IN and, if required, edit the Display Name field to update the product plugin display name.
Note: You can modify the product plugin display name only after registering the product.- Select the Register
button.
The Register Plug-in window appears. The PLUGIN HOST, PRODUCT TYPE, and DISPLAY NAME fields are auto populated. Select Register to register the product.
- Select the Unregister
button.
The Unregister Plug-in window appears. If you select Continue to unregister the product, the product plugin will be removed from the NAVIGATION panel. Also, any open panel belonging to this plugin will be closed, and changes to the product plugin will not be saved.
Note: You can also right-click on the product row and select Register or Unregister as needed to perform actions similar to those in the PLUG-IN section within the DETAILS panel. - Select the Register
- CERTIFICATE DETAILS: Select
of the CERTIFICATE DETAILS. The Proficy product certificate details, such as Issuer Name, Valid From, Valid To, and others, are displayed.
- LICENSE DETAILS: Select
of the LICENSE DETAILS. The Proficy product license details, such as License Expiration, Licensed Version, Number of OPC Connections, Number of OPC UA Server Connections, Number of Web Server Connections, and others, are displayed.
- PLUG-IN: Select